Can IBB flag in I2C status register be used to detect the End of master writing process....

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can IBB flag in I2C status register be used to detect the End of master writing process....

1,273件の閲覧回数
Chethu
Contributor I

Hi

I am using the MCF52259 controller as I2C slave for some communication, Here the master can send either read multiple bytes or write multiple bytes type of commands...I can detect read multiple byte command if i receive the repeated start condition.. but how can i detect the multiple write command i have received(here the problem is I am confused whether i can detect the end of master writing process using the IBB flag in I2C status register )..Please answer this question..

 

 

Thanks & Regards,

Chethu 

ラベル(1)
0 件の賞賛
返信
1 返信

795件の閲覧回数
Chethu
Contributor I
In relation to the above query,Suppose it takes some time to process the received data from the master and how can i inform the master about this process...by making the line busy?.. but how can i make it being the slave?
0 件の賞賛
返信