CPLD pin and the M547xEVB Lite Development Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPLD pin and the M547xEVB Lite Development Kit

3,081 Views
Linux
Contributor I
I have 2 questions about the M547xEVB Lite Development Kit.

1. If the CPLD is unprogrammed, will its pin (by default) drive the TA (transfer acknowledgment) line?

2. Is the CPLD already programmed to drive the TA (transfer acknowledgment) line?
Labels (1)
0 Kudos
Reply
1 Reply

1,516 Views
mnorman
NXP Employee
NXP Employee
The CPLD device on the FireEngine boards does not contain any CPLD code.  The CPLD is not required to run the system.  LogicPD has developed some enhanced features that use the CPLD such as a CompactFlash interface.  Consult the LogicPD documentation that came with your kit or the LogicPD web site for more details: http://www.logicpd.com
 
By default, the CPLD will not drive /TA.
 
0 Kudos
Reply