CPLD pin and the M547xEVB Lite Development Kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPLD pin and the M547xEVB Lite Development Kit

3,096件の閲覧回数
Linux
Contributor I
I have 2 questions about the M547xEVB Lite Development Kit.

1. If the CPLD is unprogrammed, will its pin (by default) drive the TA (transfer acknowledgment) line?

2. Is the CPLD already programmed to drive the TA (transfer acknowledgment) line?
ラベル(1)
0 件の賞賛
返信
1 返信

1,531件の閲覧回数
mnorman
NXP Employee
NXP Employee
The CPLD device on the FireEngine boards does not contain any CPLD code.  The CPLD is not required to run the system.  LogicPD has developed some enhanced features that use the CPLD such as a CompactFlash interface.  Consult the LogicPD documentation that came with your kit or the LogicPD web site for more details: http://www.logicpd.com
 
By default, the CPLD will not drive /TA.
 
0 件の賞賛
返信