CFLINUX_20100901_ltib.iso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CFLINUX_20100901_ltib.iso

4,197 Views
frendi
Contributor I

Hi,

 

I'm developing on a custom board derived from M54455EVB. I've seen that Freescale released new ltib distribution iso.

This iso include new kernel version (2.6.29). I would like to try, because with kernel version 2.6.25 we have some problems.

So with new iso, some packages have corrupted, mainly kernel patches. I've tried to delete this patches and forced them to download from server bitshrine.org but unsuccessfully..

 

 

Thanks for your answers.

 

Great regards.

Labels (1)
0 Kudos
Reply
8 Replies

3,146 Views
frendi
Contributor I

It seems that these patches corrupted: 

 

 

kernel-2.6.29-Add-ATA-support-for-MCF54455.patch:                            
kernel-2.6.29-Add-CAU-support-for-MCF5441x.patch:                            
kernel-2.6.29-Add-CFV4E-FPU-support-for-MCF547X_8X.patch:                    
kernel-2.6.29-Add-common-I2C-for-M5445X-M547X_8X-and-add-I2C.patch:          
kernel-2.6.29-Add-common-serial-driver-and-add-IRDA-for-m5.patch:            
kernel-2.6.29-Add-cpu-dma-sync-function-for-coldfire-platform.patch:         
kernel-2.6.29-Add-cryto-driver-for-M54451EVB.patch:                          
kernel-2.6.29-Add-dspi-driver-support-on-m5441x-platform.patch:              
kernel-2.6.29-Add-FlexCAN-driver-support-on-m5441x-platform.patch:           
kernel-2.6.29-Add-L2-switch-driver-for-Modelo-linux2.6.patch:                
kernel-2.6.29-Add-M547XEVB-and-M548XEVB-for-Linux2.6.29.patch:               
kernel-2.6.29-Add-PCI-bus-driver-for-M54455-and-M547X_8X.patch:              
kernel-2.6.29-Add-ramdisk-support-for-547x8x-boards.patch:                   
kernel-2.6.29-Add-USB-OTG-support-on-m5441x-platform.patch:                  
kernel-2.6.29-Add-vDSO-support-for-Coldfire-platform.patch:                  
kernel-2.6.29-Add-watchdog-driver-support-for-M5445X-and-M547X_8X.patch:     
kernel-2.6.29-Adjust-the-PCI-ioremap-on-M54455EVB-board.patch:               
kernel-2.6.29-back-port-the-cbs-memset-bug-for-e100.patch:                   
kernel-2.6.29-Change-some-jffs2-warning-to-debug-info.patch:                 
kernel-2.6.29-clean-up-the-bi-record-for-Coldfire-platform.patch:            
kernel-2.6.29-default-configuration-update-for-serveral-boards.patch:        
kernel-2.6.29-dma-update-for-coldfire-platform.patch:                        
kernel-2.6.29-Dummy-function-for-PCI-errata-and-PCI-workaround-for.patch:    
kernel-2.6.29-Enable-1588-functions-for-M5441x-FEC-module.patch:             
kernel-2.6.29-FEC-RMII-interface-slew-rate-setting-fix.patch:                
kernel-2.6.29-Fix-Bug-of-usb-otg-resource-register-issue-on-m5441x-2.patch:  
kernel-2.6.29-Fix-the-l2-switch-bridge-port-close-issue.patch:               
kernel-2.6.29-Fix-the-modelo-switch-port-0-down-up-issue.patch:              
kernel-2.6.29-M54418twr-default-configuration-update.patch:                  
kernel-2.6.29-M54418TWR-DSPI-driver-update.patch:                            
kernel-2.6.29-M54418TWR-software-reset-fix-for-kernel.patch:                 
kernel-2.6.29-M54455-default-config-for-kernel-2.6.29.patch:                 
kernel-2.6.29-m547x-pci-code-and-compile-warning-clean-up.patch:             
kernel-2.6.29-MMC-over-SPI-driver-update-for-M54451EVB-board.patch:          
kernel-2.6.29-Modelo-1588-irq-bug-fix.patch:                                 
kernel-2.6.29-Support-Coldfire-arch-in-linux2.6.29-1.patch:                  
kernel-2.6.29-Unclock-the-all-register-write-for-m5441x-RTC.patch:           
kernel-2.6.29-vDSO-update-on-CF-Linux-platform.patch:                        
Is there someone that tried these patches on new ltib iso CFLINUX_20100901_ltib.iso?
Thanks so much.

 

0 Kudos
Reply

3,146 Views
frendi
Contributor I

No one have problems on this iso ???

0 Kudos
Reply

3,146 Views
TomE
Specialist II

It might help if you provided more details on how they are corrupted. Is it a problem reading the files from the ISO? Are the checksums wrong? What are the symptoms of your problem?

 

Where did you download it from? Googling for the name I'm guessing you got it from

 

    http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_BSP_COLDFIRE

 

I'm not going to look at this (not using that system or board) but more details might help others recognise the problem.

 

 

 

0 Kudos
Reply

3,146 Views
frendi
Contributor I

It seems that almost all packages on iso are corrupted.The If you try to download iso and you open some kernel patch like  kernel-2.6.29-Add-ATA-support-for-MCF54455.patch, you can view that file is corrupted. It seems a general problem on iso. I downloaded iso many times, also from that url posted.

 

In my opinion problem is located in file corruption inside iso hosted on website. I downloaded iso many times, on different machine with Ubuntu 10.10, Windows7, Mac Osx Snow Leopard 10.6.4, but in every case many files inside iso are corrupted. In these conditions, when i'm installed ltib, ltib generated various errors because md5sum files check failed. So, ltib tried to download (as I think it's right) packages that in iso were corrupted. So, until to kernel package, ltib had successful to download and install packages. With kernel, instead, corrupted patches didn't exist also on server bitshrine.org , then i can't preparate kernel package.. 

 

Thanks

0 Kudos
Reply

3,146 Views
J2MEJediMaster
Specialist I

If the web site ISO image is truely corrupted, that problem needs to be reported. You can do that by submitting an on-line service request. Click here to do that. This will get the process started to fix the problem. Or, maybe they can point out what you are overlooking in the install process. (It happens.) In either case, doing that should get you going.

 

---Tom

0 Kudos
Reply

3,146 Views
frendi
Contributor I

Infact I have submitted a service request, because the problem exists. I hope that Freescale fixes it.

Anyway it worries me that within beyond 1 month nobody has reported the problem.

 

Thanks so much.

0 Kudos
Reply

3,146 Views
TomE
Specialist II

Yes, this ISO does look somewhat broken:

 

 

tevans@tome:~/.gvfs/CFLINUX_20100901_ltib.iso/pkgs$ wc ker*patch   1890    6472   53149 kernel-2.6.29-Add-ALSA-driver-support-for-MCF5445X.patch      0       0   25382 kernel-2.6.29-Add-ATA-support-for-MCF54455.patch      0       0    2078 kernel-2.6.29-Add-CAU-support-for-MCF5441x.patch      0       0     819 kernel-2.6.29-Add-CFV4E-FPU-support-for-MCF547X_8X.patch      0       0   67210 kernel-2.6.29-Add-common-I2C-for-M5445X-M547X_8X-and-add-I2C.patch      0       0    9039 kernel-2.6.29-Add-common-serial-driver-and-add-IRDA-for-m5.patch     54     188    1657 kernel-2.6.29-Add-core-watchdog-support-for-M54418.patch      0       0    1840 kernel-2.6.29-Add-cpu-dma-sync-function-for-coldfire-platform.patch      0       0   79874 kernel-2.6.29-Add-cryto-driver-for-M54451EVB.patch    474    1591   14369 kernel-2.6.29-Add-driver-to-support-ten-UART-devices-on-m5441x-pla.patch   1656    6079   44803 kernel-2.6.29-Add-DSPI-driver-support-for-MCF5445X.patch      0       0   38275 kernel-2.6.29-Add-dspi-driver-support-on-m5441x-platform.patch.../CFLINUX_20100901_ltib.iso/pkgs$ wc *patch | grep " 0 " | wc    153     612   10384tevans@tome:~/.gvfs/CFLINUX_20100901_ltib.iso/pkgs$ od zaptel-1.4.12.1-m68k-1.patch0000000 000000 000000 000000 000000 000000 000000 000000 000000*0261220 000000 000000 000000 000000 000000 000000 000000 0000000261237.../CFLINUX_20100901_ltib.iso/pkgs$ file ker*patch | grep data | wc     38      76    3078(they should be showing up as "ASCII English text" like the other patches in here).../CFLINUX_20100901_ltib.iso/pkgs$ od -c *Unclock*0000000  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0  \0*0004420  \0  \0   0   8   b   b   3   b   7   3   9   1   3   2   b   10004440   f   1   5   5   2   6   a   d   1   4   6   4   5   3   4   b0004460   9   b           k   e   r   n   e   l   -   2   .   6   .   20004500   9   -   U   n   c   l   o   c   k   -   t   h   e   -   a   l0004520   l   -   r   e   g   i   s   t   e   r   -   w   r   i   t   e0004540   -   f   o   r   -   m   5   4   4   1   x   -   R   T   C   .0004560   p   a   t   c   h0004565

 Many of the files are empty. Others have large blocks of zeros followed by "something".

 

0 Kudos
Reply

3,146 Views
Groleo
Contributor I

What I did was get the corrupted patches from  http://www.bitshrine.org/gpp/

Some of them I couldn't find and I guess freescale didn't bothered to upload them. I've posted a ticket and I'm waiting now.

 

kernel-2.6.29-Add-FlexCAN-driver-support-on-m5441x-platform.patch
kernel-2.6.29-Add-common-I2C-for-M5445X-M547X_8X-and-add-I2C.patch
kernel-2.6.29-Add-cpu-dma-sync-function-for-coldfire-platform.patch
kernel-2.6.29-Add-watchdog-driver-support-for-M5445X-and-M547X_8X.patch
kernel-2.6.29-Dummy-function-for-PCI-errata-and-PCI-workaround-for.patch
kernel-2.6.29-Fix-Bug-of-usb-otg-resource-register-issue-on-m5441x-2.patch
kernel-2.6.29-MMC-over-SPI-driver-update-for-M54451EVB-board.patch
kernel-2.6.29-Unclock-the-all-register-write-for-m5441x-RTC.patch
kernel-2.6.29-default-configuration-update-for-serveral-boards.patch

 

0 Kudos
Reply