CF Flasher for M52259?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CF Flasher for M52259?

7,140 Views
mjbcswitzerland
Specialist V

Hi All

 

Does anyone know whether there will be a new release of the CF Flasher to support programming the Kirin3 - M5225x devices?

 

Regards

 

Mark

Labels (1)
0 Kudos
Reply
7 Replies

4,476 Views
HLaidet
Contributor I

 

Hello
i use CFFlasher V3.1.10 and PE_USB_ML
the algo for MCF52259 is "CFM(512).alg" it is already in "CFFlasher\alg".
you only have to generate the config file for your board.
i generated "DigibutlerK3.cfg" for my board (MCF52259).
using internal oscillator when starting
CLKMOD0=0 (pull-down), CLKMOD1=0 (pull-down), XTAL=1 (10k pup resistor).
Regards,
Henri

 

0 Kudos
Reply

4,475 Views
RuiFaria
Contributor III

Hi Henri,

 

Did you try to use CFFlasher by command-line?

 

I only can use it by GUI! :smileyfrustrated:

 

Best Regards,

Rui Faria

0 Kudos
Reply

4,475 Views
tr111
Contributor I
if your are the utasker's mark!
email to me [email protected]
I will give you the file,I have finished the CF Flasher config for the mcf52259!
Because I use you utasker and your are very good at the utasker about the coldfire!
0 Kudos
Reply

4,476 Views
alager
Contributor II

Is CF Flasher being given out for the 52259?  It's obvious that there is a version that was given to the uTasker guy, how about the rest of us that find the utility extremely useful and are moving on to bigger/newer chips?

 

Thanks,

Aaron

0 Kudos
Reply

4,476 Views
bkohan
Contributor II

tr111,

Can you share this 52259 algorithm with the commnity?  I would like to use it.

 

Thanks,

 

B.K.

0 Kudos
Reply

4,472 Views
ssinfod
Contributor IV

Here are the files. (see attached zip).

Maybe it could be useful for somebody !

0 Kudos
Reply

4,474 Views
tr111
Contributor I
No! you must do yourself!
or the CodeWarrior IDE have the flash programmer!
0 Kudos
Reply