CF Flasher - Could not initialize BDM device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CF Flasher - Could not initialize BDM device

6,049 Views
skenaka
Contributor I
Hi
 
I have M52235EVB and CW6.3 installed. I can compile "Hello World" code and download and debug it through USB_ML_CFE rev.C in CW without a problem. However, when I try to use CF Flasher(3.1) to write the NicheLite S19 code to the board, it complains "Could not initialize BDM device."
  • Target configuration is set to M52235EVB and BDM Communication is set to PE_USB_ML,a nd others remain defaults
  • Updated the driver to the latest one (windrvr6.sys ver.7.0.0, 3/21/05) from P&E, passed the P&E's test
  • Works fine with CW
  • Not using CW and CF Flasher at the same time, even tried right after a reboot
Any idea where might be the problem?
Thanks,
 
- skenaka
 
Labels (1)
0 Kudos
Reply
2 Replies

2,326 Views
skenaka
Contributor I
Hi Stan
 
Problem solved. Thanks a lot!
 
I found two files with the same file name in 'CW\bin' and 'CW\Third_party\CF_Flasher' directories, but not in seperately installed CF Flasher directory. So probably should copy the unit_cfz.dll to the new CF Flasher directory. (copy to system32 works fine, too!)
 
Thanks again.
 
- skenaka
0 Kudos
Reply

2,326 Views
Stan
Contributor I
try to add this dll in windows\system32
 
Regards,
 
Stan
 
Message Edited by t.dowe on 2009-10-21 02:38 AM
0 Kudos
Reply