Booting UClinux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting UClinux

2,422件の閲覧回数
cfernandez
Contributor I
Hi!

I'm trying to boot an uClinux from NAND Flash on a M5329EVB. I copy the uImage in NAND FLash using the nandwrite aplicattion on a kernel loaded in RAM.

When  I restart u-boot i try to boot from nand (nbood 0x40020000 0 0) uncompressing the image on RAM. Kernels starts to boot but stops at:

Loading from NAND 16MiB 3,3V 8-bit, offset 0x0
   Image Name:   Linux Kernel Image
   Created:      2008-12-09   9:35:12 UTC
   Image Type:   M68K Linux Kernel Image (gzip compressed)
   Data Size:    1600436 Bytes =  1.5 MB
   Load Address: 40020000
   Entry Point:  40020000

(STOP)

and then u-boot takes control again?

Any one knows what is happening on this M5329EVB board?

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,455件の閲覧回数
J2MEJediMaster
Specialist I
Check out FAQ-28617 which has some tips on moving the rootfile system to NAND memory for a similar board (5373EVB). It may give you enough information to sort out the problem. HTH.

---Tom
0 件の賞賛
返信

1,455件の閲覧回数
cfernandez
Contributor I
Thanks, but the problem is not mounting a JFFS2 system in my NAND flash.

I would like to get to partitions in flash one for the kernel and other for the filesistem. Any one knows the clue to part it? I'm using u-boot-2008.10 but i can't activate the mtdparts command


Message Edited by cfernandez on 2008-12-10 08:20 AM
0 件の賞賛
返信