Booting Linux from the M5475EVB's builtin flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting Linux from the M5475EVB's builtin flash

1,635 次查看
NCommander
Contributor I
I've recently acquired a M5475EVB secondhand from another developer on my team, and I'm working to get Linux and its initrd burnt onto the firmware. I don't have the BDM module, or the cable for this board so I'm unwilling to remove dBUG as I'm likely to make a brick if I tried to replace it with u-boot.

Currently, I've determined the m5475EVB has two flash chips, a small 2MB one which currently only houses dBUG, and the larger 16MB one that Linux properly sees (the 2MB one isn't seen AFAIK, as the fl reports both, but Linux only reports 16MB of flash). I want to use mtdparts to parition the 16MB chip into smaller chunks, 4MB for the kernel, 4MB for initrd, and 8MB of flash for the userland (although ATM, the 4MB initrd is only going to be used to load a RAMdisk so I can format the 8MB flash to JFFS2).

In general, is there any good notes or documentation on doing such a thing, or anyone have experience on using mtdparts?
标签 (1)
0 项奖励
回复
1 回复

1,041 次查看
J2MEJediMaster
Specialist I
Try looking at FAQ-28617, which describes configuring an 5373EVB board to boot from its large NAND memory part. It's not the same ColdFire processor, but maybe the information will help get you started.

---Tom
0 项奖励
回复