Boot loader for 5251

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot loader for 5251

3,493 次查看
Lord_Avon
Contributor I
Dear all,
 
 I'm interested in finding out if it's possible to get a boot loader for the 5251 eval board. It has no network card, so booting from a network device is a no go. But it does have an SD card slot.
 
 What I'd *LOVE* is to be able to build a linux filesystem on an SD card, pop it into the 5251 board and then get the bootloader in flash to boot from it and load up my newly compiled/tweaked linux system.
 
 This *should* be possible shouldn't it? or is this never going to happen?
 
 If not, is there another way of getting a new build of an OS into the board other than through serial? the 15-20 minute wait for download each time I want to test is a *REAL* pain.
 
Paul
标签 (1)
0 项奖励
回复
4 回复数

2,295 次查看
ShenLi
Contributor I
Hi,Paul
Yes, the dBUG boot linux from serial com is painful, but it is only for development stage. The dBUG support gzip file and allow you store your linux gzip image into the flash. And everytime power up the board, the dBUG can unzip the image into sdram and run it. I do not know if it can release your pain.
0 项奖励
回复

2,295 次查看
Lord_Avon
Contributor I
Shen,

 Many thanks, I guess for the moment that will be good enough.
Is there a way of mounting an SD card using the current Linux BSP? I assume it can be mounted just like a standard ATA device?

Paul
0 项奖励
回复

2,295 次查看
ShenLi
Contributor I
Paul
I am afraid M5251 does not have SD Linux Driver currently. But we do will release the driver for it .
 
Shen Li
0 项奖励
回复

2,295 次查看
Lord_Avon
Contributor I
Please let us (and me) know when this is done.
i was going to try the 5445 linux, but I've not been able to download it.

Many thanks,
Paul
0 项奖励
回复