Backup Watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Backup Watchdog

1,827 Views
Dekabrist
Contributor I

Hello, all

 

My board run under BDM and Backup Watchdog Timer init with Processor Expert bean. But, when I break debug (stop Run) Backup Watchdog Timer NOT reset MCU and I read WCNTR = 0000, even when my programm write 0x5555 0xAAAA to WSR. My configuration:

CLKMOD[01] = 01 (CLKMOD0 pin have pullup resistor, XTAL pin NOT have pullUP resistor)

BWCR (CLOCK MODULE) = 0x00 - 32 MHz from bus

WCR = 0x0003

WMR = 0xFFFF - 8388,48 ms timeout

 

Init function:

 

void Wtm1_Init(void)

{

  /* WMR: WM=0xFFFF */

  setReg16(WMR, 0xFFFFU);              

  /* WCR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,STOP=0,WAIT=0,DOZE=0,??=1,EN=1 */

  setReg16(WCR, 0x03U);                

}

 

Can I check software reset in the debug mode?

 

P.S. I use CW version 5.9.0 build 5293

 

Thank for answer

Labels (1)
0 Kudos
Reply
2 Replies

1,656 Views
DavidS
NXP Employee
NXP Employee

Hi Sergey,

The ColdFire BWT is good for production application but not good for debugging mode.  The BWT clock continues clocking even when you hit a breakpoint (which stops the core but it not the same as implementing a STOP instruction).

You could use the internal (slower) clock rather than the 32MHz to increase the timeout period.

Regards,

David

0 Kudos
Reply

1,656 Views
Dekabrist
Contributor I

Hi David

I activate toolbutton "break " in the debug mode and wait more than BWT timeout - BWT must reset MCU under this conditions? I make sure that my BWT work.

Sergey


0 Kudos
Reply