About MCF5482 SPI to USB solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MCF5482 SPI to USB solution

1,822件の閲覧回数
Jason_Shi
Contributor I

I want to connect a USB host to my MCF5482 platform via a MAX3421, the interface is SPI, the MAX3421 support spi clk up to 26M, and suport full speed USB host 12M bps.

 

Is there any one used MCF54xx like this? I want to know how fast it is up to, I think it is impossible to reach 12M bps.

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

1,138件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi,

 

The DSPI module on MCF54xx can attain up to 25MHz and also you can use the eDMA module to reduce CPU load, I think with 26MHz SPI on MAX3421, it can satisfy the requirements for USB 12Mbps.

 

By the way, you are not supposed to attain 12Mbps any way, it's just a theoratical value.

0 件の賞賛
返信