AN3038 using EMAC Unit / verifying ECDSA Signature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN3038 using EMAC Unit / verifying ECDSA Signature

978 次查看
chbecker
Contributor II

Dear Community,

 

currently im implementing ECDSA key verifying algorithm on a mcf51qm128 coldfire controller. Unfortunately my first implementation using pure c language and parts of the GMP Library makes it very slow, so I have to improve my algorithm.

 

Therefore I found the application not an3038 which handles multiplying using EMAC unit.I would need some support how I implement this assembly function in my c project (codewarrior development studio 10.2).

 

I create the mp_mul64.c and mult_add64.s File. But when im trying compile it I get the following error:

Instructions must occur within code section    "mul_add64.s"   

 

Is there anything I have to observe when using assembly code in c project or maybe there already exists any implemantion for verifying an ecdsa signature on coldfire platform ?

 

 

Thanks for help

 

Yours sincerely

 

 

Christian Becker


标签 (1)
标记 (4)
0 项奖励
回复
0 回复数