68000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

68000

13,203 Views
dragomil
Contributor I
I have acquired some MC68000 64pin microprocessors.
 
Can anybody help with a test circuit for these, and perhaps any software needed to run the tests ?
Labels (1)
0 Kudos
Reply
6 Replies

6,153 Views
Alban
Senior Contributor II
Hi mimil,

To help you, we need at least the following info:
Which tests are you talking about ?
What is the exact reference of the microprocessor (markings on it) ?


Cheers,
Alban.
0 Kudos
Reply

6,153 Views
dragomil
Contributor I
 Hi Alban,
 
I have a number of them with different markings. Two of them are 10 MHz types, marked as follows,
 
MC68000P10
2C91E
OEBV9214
 
As far as tests are concerned, I just want to make sure they are working ok.
 
Regards    Dragomil
0 Kudos
Reply

6,153 Views
Alban
Senior Contributor II

Hi,

Looking round, I found these documents.
The MCU is older than I am :smileytongue:

The Freescale Hibbert website is quite good to find old datasheet and all.

http://merchant.hibbertco.com/fs11/freescale/an1123.fsl.d.rev0.pdf
http://merchant.hibbertco.com/fs22/pdf-docs/freescale/mc68000.fsl.ac.rev3.pdf
http://merchant.hibbertco.com/fs13/freescale/ar235.fsl.d.rev0.pdf
http://merchant.hibbertco.com/fs13/freescale/ar235.fsl.d.rev0.pdf
http://merchant.hibbertco.com/fs22/pdf-docs/freescale/dce406.fsl.d.rev0.pdf

Semiconductors have a shelf life. If yours were not kept in a moist free bag, it would affect their life span.
Also, I can only recommend to change to a newer generation if you can. Especially with the free sample programme, you don't have to pay !

Cheers,
Alban.

Message Edited by Alban on 01-31-2006 10:11 AM

0 Kudos
Reply

6,154 Views
dragomil
Contributor I

Okay Alban,

 

I will have to test them for exposure to silica gell.

Regards  dragomil

0 Kudos
Reply

6,154 Views
Nabla69
Contributor V
Funny you should talk about these !
A new datasheet is just available :smileytongue:
http://www.freescale.com/files/32bit/doc/ref_manual/MC68000UM.pdf
Cheers, A.
0 Kudos
Reply

6,154 Views
dragomil
Contributor I

MC68HC705 with external EPROM ?

Alban (Moderator) moved this message with a new question to a more appropriate location.

Follow link to see

Message Edited by Alban on 02-02-2006 01:51 PM

0 Kudos
Reply