68000 interrupt acknowledge cycle duration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

68000 interrupt acknowledge cycle duration

5,950件の閲覧回数
CharlesM
Contributor I
I'm working with a MC68000 based system where the interrupt acknowledge cycle for autovectored interrupts seems to be taking a variable amount of cycles (26/32/44) rather than the 44 cycles listed in the 68000 manual. I'd like to know exactly what defines the cycle duration.

First, some background on the circuit: A periodic interrupt occurs which asserts /IPL2 through /IPL0 accordingly to request a level 1 interrupt. When /AS goes low and FC2,FC1,FC0 are high, /VPA is pulled low. It remains asserted until any of /AS or FC2,FC1,FC0 are negated. The 68000 always terminates the cycle by pulling /AS high after the variable cycle delay; this isn't an issue of /VPA being negated too early.

I get a shorter cycle time depending on what the 68000 is doing; e.g. executing NOPs gives 26 cycles, waiting in a STOP #$2000 condition tends to give 32 cycles, and so on.

I've monitored all the other signals and there seems to be nothing that would impact the timing, I'm assuming this is some kind of internal decision the 68000 makes. But I don't know the criteria involved.

The exact timing for an interrupt acknowledge cycle looks like this:

1. Finish executing current instruction
2. Stack PCL at SSP-2 (8 cycles for RAM access)
3. Interrupt acknowledge cycle (26/32/44 cycles, variable)
4. Stack SR at SSP-6 (8 cycles for RAM access)
5. Stack PCH at SSP-4 (8 cycles for RAM access)
6. Read interrupt vector low word (10 cycles for ROM access)
7. Read interrupt vector high word (10 cycles for ROM access)
8. Execute first instruction from ISR

My concern is that the the periodic interrupt has some jitter introduced between each interrupt as the the time is off by a variable amount of cycles per interrupt, which I need to eliminate.

Rather than rework the design I'd like to know why the 68000 does this even if it's a limitation of the CPU and something I can't control. (for example, maybe the specification of 44 cycles indicates a maximum; rather than the absolute count?)
ラベル(1)
0 件の賞賛
返信
1 返信

4,279件の閲覧回数
hmsmith
Contributor I
In a 68000 system the E clock (originally the cycle clock for the 6800 CPU) is generated by dividing the system clock by 10 - the E clock was low for six clocks and high for four clocks. At the original 68K speed of 10 MHz this gave a suitable 1 MHz clock for 6800 peripheral devices.

When the VPA signal is activaated in response to a external cycle, the CPU will synchronize to the E clock and terminate the cycle after the next active E clock.

Since your interrupt is not synchronized to the E clock, there is a random delay based on the state of the E clock when the interrupt acknowledge occures.

Regards,

Hugh
0 件の賞賛
返信