5282Lite EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5282Lite EVB

1,770件の閲覧回数
Mikeeulkeul
Contributor I
Hello,

I'm having some difficulty communicating with the pc so i was wondering if one of you maybe had a little exemple of a program that was working with the ethernet module so I could try it and know if the problem comes from my program or from the dsp like I had some problem with it before.

Thanks in advance.
ラベル(1)
0 件の賞賛
返信
1 返信

1,132件の閲覧回数
Alessandro
Contributor I
Dear Mike,

I'm experiencing the same problem as you. I'm not able to communicate
with the PC using the embedded DBUG command "dn". The strange thing is
that no frames are sent from the board when the command is launched
(I'm sure because I have checked with a network analyzer). For my
case, it seems to be a transceiver problem. Connected to my PC directly,
the CML board is not able to establish a reliable link with it because
sometimes the link goes down.

If you find something about this issue please let me know (alessandro.
[email protected])

Best regards

/Alessandro
0 件の賞賛
返信