52259 wont boot without bdm attached?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

52259 wont boot without bdm attached?

1,569件の閲覧回数
Byra
Contributor I

Ive got a 52259 on a custom board that boots and runs fine from codewarrior with the bdm attached. However, when I remove the bdm and reset the board, it doesnt run. Im using a 48mhz crystal and it should work with clkmod0 and 1 pulled up to vcc. However, have tried all configurations of clkmod0 and clkmod1 with no luck. When I try the same code on the tower board, it works find and boots up with or without the bdm attached. I have the same 4 pins pulled upon my bdm connector as on the tower board. Im using the same crystal as on the tower board. I dont get it. Im sure its something obvious, but I cant find it.

 

Thanks for any help!

 

--Byra

ラベル(1)
0 件の賞賛
返信
1 返信

1,176件の閲覧回数
scifi
Senior Contributor I

It could be the same problem as this:

 

https://community.freescale.com/message/65237#65237

0 件の賞賛
返信