52252 powerfail detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

52252 powerfail detection

1,926件の閲覧回数
LPs1978
Contributor III

Hi all,

   I'm designing a new low cost application and I need to save some data in a falsh sector when power fails.

I have questions:

  • it's ok to use the LVD interrupt to start the flash save procedure? What is the VDD minimum that cause the interrupt (threshold)?
  • This interrut can leave me time enough to write a flash sector?


The not so low cost solution is to have an external circuit connected to an IRQ pin that allow me to define the threshold.

 

Are these available solutions or someone had some different ideas?

 

Thaks in advvance.

Message Edited by LPs1978 on 2009-03-24 10:48 AM
Message Edited by LPs1978 on 2009-03-24 10:48 AM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,234件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

This topic is being discussed here:

http://www.utasker.com/forum/index.php?topic=549.0

 

Maybe that will help you.

 

Regards

 

Mark

 

www.uTasker.com

 

 

Message Edited by mjbcswitzerland on 2009-03-24 02:21 PM
0 件の賞賛
返信

1,234件の閲覧回数
RichTestardi
Senior Contributor II

I also would be concerned with the supply voltage being so far out of spec when the lvd interrupt occurs to try and get any meaningful work done (even if the supply came back!), much less manipulate flash...

 

What we have done in the past is set up a resistor divider on the *pre* regulated supply voltage (dividing it to within spec of the a/d converter), and then we can watch as it drops below the regulators drop-out voltage, and thereby get our meaningful work done before the supply voltage is out of spec.

 

-- Rich

 

0 件の賞賛
返信