5207 Chip configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5207 Chip configuration

2,573件の閲覧回数
AndyDaytona
Contributor I
Hello,
 
I am currently moving our design from the 5206e to the 5207 and I have a question
about the chip configuration module.
 
I look at the schematics of the evaluation board and I see that the configuration
bits are set using a latch connected to the bus.
 
Is it not possible to use pull ups and downs directly connected to the data bus to
configure the chip? Or is there some problem that I'm not aware of?
 
My bus is already heavily loaded with memory and devices so I am hoping to get rid of this extra load.
 
best regards
Andy
ラベル(1)
0 件の賞賛
返信
1 返信

1,350件の閲覧回数
timotay01
Contributor I

Your using /RCON pin in conjunction with your resistors? See "Reset Configuration" (Section 9.4.1 in the spec I have).

0 件の賞賛
返信