2 new appnote to help with ColdFire TCP/IP stack and HTTP server - AN3455  and AN3470

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2 new appnote to help with ColdFire TCP/IP stack and HTTP server - AN3455  and AN3470

9,620 Views
ericgregori
Contributor I
0 Kudos
Reply
5 Replies

3,248 Views
ericgregori
Contributor I
AN3470 Firmware
 
 
 
Use the link above to download the ColdFire TCP/IP stack with examples.  This firmware is the firmware described in the AN3470 appnote.
 
 
Projects included in the build:
 
web server
UDP server
UDP client
TCP server
TCP client
Serial to Ethernet server/client
TCP client based multi-node alarm system
Applications/utilities for TCP and UDP performance measurement
TFTP server examples
DHCP examples
 
 
 
0 Kudos
Reply

3,248 Views
Petter_fupp
Contributor I
Thanks, Eric!

This was increadably helpful. Would have been even more helpful if I had it a while ago -but I still found usefulness in memory saving stuff, etc.

I think this post should be made sticky, to stay on top in the forum.

Cheers,
Petter
0 Kudos
Reply

3,248 Views
Jack_
Contributor I

I have downloaded the stack example AN3470SW.zip and try to compile directly with CodeWarrior 6.2

I get a lot of errors like:

            - Instruction not legal for current target processor(s)

            ......

            - internal compiler error (report to [email protected])

            while executing in file ‘PCodeAssembly.c’ line: 626

            (compiling ‘_printk_mknumstr’ in ‘printf.c’)


            - the file ‘Int_hnadlers.h’ cannot be opened

            Int_handlers.c line 12 #include “Int_handlers.h”
            .
            .
            .
            Etc
 

I suppose that the problem is that CodeWarrior 6.2 doesn’t support the MCF5223x microcontrollers. 

Can you tell me please if this is true? 

If is true, what version I must use?

There is some example to run this code on MCF5208EVB or the steps to follow?

Thanks,

Jack

0 Kudos
Reply

3,248 Views
MasterDanilo
Contributor I

Hi man...

 

Codewarrior 6.x are only for coldfire v1 microcontrollers... For the V2 family you must use Codewarrior 7.x or the new Codewarrior 10.x (eclipse based) that attends coldfire v1,v2,v3 and v4.

 

Best reguards...

 

Danilo Pagano

0 Kudos
Reply

3,248 Views
Kremer
Contributor I
 Can I use this code as part of my product´s project? I already read the 2 pdf´s and i see you wrote it´s intended to help coldfire customers to develop their products. So i understand i can use it and modify it as i want to incorporate it into my products using MCF52235CAL60. It´s very important to know this, because i already made a lot of modifications including POST method, Basic Authentication and so on...
0 Kudos
Reply