script executing without CW starting(excuse me for mistake)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

script executing without CW starting(excuse me for mistake)

ソリューションへジャンプ
1,982件の閲覧回数
s_kalop
Contributor I

Hello.

I want to load and start program for MSC8156ADS without starting CW. Can i execute *.tcl-script(intended for Debugger Shell originally) in windows command line without CW starting?. Can i use debugger without IDE starting, just by comman line control?

Thank you.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,822件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

0 件の賞賛
返信