bootloader in msc8151

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bootloader in msc8151

1,580 Views
David_usami
Contributor I

Initially, I want to boot MSC8151 from RapidIO mode. In our board, the host external device is a FPGA chip. Here I have a big trouble in RapidIO boot mode because FPGA fail to initialize the RapidIO port.  I doubt that the bootloader in DSP may not run. Up to now, I am not sure if the bootloader is runing.    I have configured RCW as RapidIO boot mode, where RCWLR = 32'h02230000, RCWHR = 32'h01c01e10.  I wonder how I am able to judge if the bootloader in 8151 starts to run when I power on.   Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,402 Views
lunminliang
NXP Employee
NXP Employee

Please kindly refer to SR 1-1263920098.

0 Kudos
Reply