any reference code of serial rapidIO for MSC8151?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

any reference code of serial rapidIO for MSC8151?

ソリューションへジャンプ
2,307件の閲覧回数
David_usami
Contributor I

I am a newbie for freescale StarCore DSP.  Now I want to set up serial rapidIO between MSC8151 and an FPGA.   I firstly want to configure serial rapidIO registers in MSC8151, and started setting up a loopback connection inside the DSP processor.  But looks like it does not work as expected,  DST address cannot receive any data.  The following is the code.  Anyone can help me fix it?   Thanks!

 

int main()

{

    UINT32 i;

    INT32  bdid;             // Target device id

 

    /* configure SRIO ports */

    MEM_WRITE32(RIO_P0CCSR,    0x50e00001);   // Disable SRIO

    MEM_WRITE32(RIO_P0ADIDCSR, 0x80010000);   //alternate device id

    MEM_WRITE32(RIO_P0ESCSR,   0xffffffff);   // Reset status register

     

    if(1)   // loopback

        MEM_WRITE32(PHY0_SRDSCR2, 0x008020c0);  // enable loopback

    else           // back-to-back

        // lane E/F transmitter equalization selection bus

        MEM_WRITE32(PHY0_SRDSCR1, 0x11006630);  // 1.33x relative amplitude

   

    // disable SERDES1 SRDSCR2

    MEM_CLR_BITS32(HSSI_CR1, 0x00000001);

   

    MEM_WRITE32(RIO_P0CCSR, 0x50600001);   // Enable SRIO (4x)

       

    //---------------------------------

    for(i=0;i<1024;i++)

    {

        *(UINT32 *)(SRC_ADDR+i) = i;

  

    }

    memset((void *)DST_ADDR, 0, 1024);

 

   // checking that 4 lanes are synchronized and aligned

    if(MEM_READ32(RIO_P0SLCSR) != 0xF0800000)

    {

        asm(" debug");

    }

 

    MEM_WRITE32(RIO0_BDIDCSR, 0x00FF0000);        //configure as agent

   

    MEM_WRITE32(RIO0_PGCCSR,  0x40000000);  // set device as initiator (master)

 

   // Configure Delta Outbound Address Translation Management Unit

    bdid = 1 << SHIFT22;

   

    MEM_WRITE32(RIO_P0ROWBAR1,  (1<<20)|(DST_ADDR >> SHIFT12));   // +1

    //MEM_WRITE32(RIO_P0ROWTAR1,  (2<<20)|bdid | (DST_ADDR >> SHIFT12));      // target device id << 22

    MEM_WRITE32(RIO_P0ROWTAR1,  bdid | (DST_ADDR >> SHIFT12));      // target device id << 22

    MEM_WRITE32(RIO_P0ROWAR1,   0x8004000f | (SWRITE << SHIFT12));  // for nread, nwrite

    MEM_WRITE32(RIO_P0ROWTEAR1, 0x00000000);                        // large mode device id

 

    // Configure Delta Inbound Address Translation Management Unit

    // delta 1 goes to mbus 1 [by default value of RIO_P1RIWAR0 ] and delta 0 goes to mbus1 [RIO_P0RIWAR1]

    MEM_WRITE32(RIO_P0RIWAR1, 0x8014400f);                  // all the write should go through O2M1

    MEM_WRITE32(RIO_P0RIWTAR1, (DST_ADDR >> SHIFT12));

    //MEM_WRITE32(RIO_P0RIWBAR1, (2<<20)|(DST_ADDR >> SHIFT12));

    MEM_WRITE32(RIO_P0RIWBAR1, (DST_ADDR >> SHIFT12));

 

#ifdef LATE_ARBITRATION

    MEM_WRITE32(GCR_GCR12,    0x000100ff);                  // weighted/late arbitration in RIO

#endif

 

     //---------------------------------   

    // Configure O2M

    MEM_WRITE32(RIO0_O2MCR, 0x01050000);                    // max burst size 64B

 

    // Configure OCNDMA Address Translation Management Unit

    MEM_WRITE32(RIO0_D2O_LAWBAR0, SRC_ADDR >> SHIFT12);

    MEM_WRITE32(RIO0_D2O_LAWAR0,  0x80b0000f);              // OCN to MBus Bridge 0

   

    MEM_WRITE32(RIO0_D2O_LAWBAR1, (1<<20)|(DST_ADDR >> SHIFT12));   //+1

    MEM_WRITE32(RIO0_D2O_LAWAR1,  0x80c0000f);              // RapidIO Delta Port 0

 

    //config channel 0

    *((UINT32 *)0xFFFA8110) = 0x00040000;// source attributes

    *((UINT32 *)0xFFFA8114) = SRC_ADDR;

    *((UINT32 *)0xFFFA8118) = 0x40040001;// destination attributes   +1

    *((UINT32 *)0xFFFA811C) = DST_ADDR;

    *((UINT32 *)0xFFFA8120) = 32123;

    *((UINT32 *)0xFFFA8100) = 0x0f00004;       //MR

 

    asm(" debug");

    *((UINT32 *)0xFFFA8100) = 0x0f00005;       //enable channel 0

    //*((UINT32 *)0xFFFA8180) = 0x0f00005;       //enable channel 1

    asm(" syncio");

    MEM_WRITE32(RIO_P0SLEICR,  0xF0000001);   //alert for testing, inject error *********************

    for(i=0; i<1000000;i++)

    {

        asm(" nop");

    }

    asm(" debug");

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,044件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi David,

can you help me with this questions so I can help you with this issue please:

  1. Which software are you using?
  2. What do you mean that it is not working as expected?
  3. What exactly are you doing?  What do you mean that the DST address cannot

    receive any data?

4. Which version of the SDOS tools are you using?

Any more information can be greatly appreciated.

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,045件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi David,

can you help me with this questions so I can help you with this issue please:

  1. Which software are you using?
  2. What do you mean that it is not working as expected?
  3. What exactly are you doing?  What do you mean that the DST address cannot

    receive any data?

4. Which version of the SDOS tools are you using?

Any more information can be greatly appreciated.

Regards,

0 件の賞賛
返信