WIndows 7 drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,204件の閲覧回数
Nimeshc
Contributor I

Hi

I am currently using CW 10.1 for MSC8156 development. I am planning to upgrade my windows xp to windows 7. So my question is does the usb tap have drivers for windows 7? Or is windows 7 not supported?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,903件の閲覧回数
CrasyCat
Specialist III

Hello

 

  I would recommend you to upgrade to a more recent release of CodeWarrior.

 

  Windows 7 is supported in CodeWarrior for Starcore v10.2.5 and higher.

  All drivers are then available for Windows 7.

 

  I would recommend you to upgrade to the current version of CodeWarrior for StarCore.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,904件の閲覧回数
CrasyCat
Specialist III

Hello

 

  I would recommend you to upgrade to a more recent release of CodeWarrior.

 

  Windows 7 is supported in CodeWarrior for Starcore v10.2.5 and higher.

  All drivers are then available for Windows 7.

 

  I would recommend you to upgrade to the current version of CodeWarrior for StarCore.

 

CrasyCat

0 件の賞賛
返信