Smart DSP OS for MSC8157

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Smart DSP OS for MSC8157

ソリューションへジャンプ
2,489件の閲覧回数
jiboy
Contributor I

Hi,

   I have a concern about the SmartDSP OS that is built in into the CW v10.1.8. I am trying to simulate a HW peripheral on MSC8157 which is documented to be supported on CW v10.1.8. But looks like i dont have any option to enable the Smart DSP OS while building a MSC8157 project for simulation. With this limited feature, I cannot enable any HW related functions like DMA or ETHERNET on MSC8157.

   Can you please advice how this can be addressed?

Or is there a newer version of SmartDSP for MSC8157?

 

Thanks,

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,918件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi,

 

You need to install the CW10.1.10 in order to have MSC8157+SmartDSP OS support.

The latest SmartDSP OS is B03.09.03 which incorporates alpha supprt for MSC8157 DSP on the ADS.

 

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,919件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi,

 

You need to install the CW10.1.10 in order to have MSC8157+SmartDSP OS support.

The latest SmartDSP OS is B03.09.03 which incorporates alpha supprt for MSC8157 DSP on the ADS.

 

Best regards,

Daniel

0 件の賞賛
返信