SRIO ID MSC8156

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,090件の閲覧回数
Kirill
Contributor I

Hello!

 

I could not find attribute to change SRIO ID from 16 bits to 8 bits,  what fucntion should I use or sructure?

 

Thank you!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,738件の閲覧回数
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,739件の閲覧回数
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

0 件の賞賛
返信