SRIO ID MSC8156

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRIO ID MSC8156

Jump to solution
2,151 Views
Kirill
Contributor I

Hello!

 

I could not find attribute to change SRIO ID from 16 bits to 8 bits,  what fucntion should I use or sructure?

 

Thank you!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,799 Views
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

View solution in original post

0 Kudos
Reply
1 Reply
1,800 Views
Jim95
Contributor III

Hello,

 

To switch between the 8 or 16 bits mode, you to change the CTLS bit in the RCWHR register, but must do it when the board is off.

 

Regards

 

Jimmy

0 Kudos
Reply