Profiling on StarCore 8101/8122 family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Profiling on StarCore 8101/8122 family

2,857 Views
vinod_TEL
Contributor I

Hello,

 

  I'm using the following configuration:

    a. CodeWarrior ver 3.0 (and) 3.2.2

    b. 8101ADS/8122ADS development boards

 

I'm unable to profile projects built for both these boards. This is what i notice:

 

   Target settings panel (project settings)->Debugger->Profiler->Profile Type [On Host] does not enable "Use Profile Triggers" tab {the tab is greyed out}.

   However, if I change, Target settings panel (project settings)->Debugger->SC Debugger Target->Target, to 8144, then the Profile Type [On Host] enables the said tab.

 

  So, the basic question here is: Does 8101/8122 support profiling on this version of Code Warrior?

Regards,

Vinod

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,887 Views
CrasyCat
Specialist III

Hello

 

Profiling is only available for MSC8144.

 

CodeWarrior uses VTB to collect trace information for the profiler. There is no VTB on MSC8122 or MSC8101.

 

CrasyCat

0 Kudos
Reply