Profiling on StarCore 8101/8122 family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Profiling on StarCore 8101/8122 family

2,856件の閲覧回数
vinod_TEL
Contributor I

Hello,

 

  I'm using the following configuration:

    a. CodeWarrior ver 3.0 (and) 3.2.2

    b. 8101ADS/8122ADS development boards

 

I'm unable to profile projects built for both these boards. This is what i notice:

 

   Target settings panel (project settings)->Debugger->Profiler->Profile Type [On Host] does not enable "Use Profile Triggers" tab {the tab is greyed out}.

   However, if I change, Target settings panel (project settings)->Debugger->SC Debugger Target->Target, to 8144, then the Profile Type [On Host] enables the said tab.

 

  So, the basic question here is: Does 8101/8122 support profiling on this version of Code Warrior?

Regards,

Vinod

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,886件の閲覧回数
CrasyCat
Specialist III

Hello

 

Profiling is only available for MSC8144.

 

CodeWarrior uses VTB to collect trace information for the profiler. There is no VTB on MSC8122 or MSC8101.

 

CrasyCat

0 件の賞賛
返信