Problem loading MSC8156ADS board with cw 10.2.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem loading MSC8156ADS board with cw 10.2.9

ソリューションへジャンプ
2,794件の閲覧回数
hemah
Contributor I

Im getting follwing error while i am trying to load a application in MSC8156ADs board using cw 10.2.9

Failed to resume target process., CCSProtocolPlugin : Could not connect to the probe (or other debug link)

 

The same application is loading without any error when i tried with cw 10.1.1

whether there is any settings that is to be changed in debug configurations while loading with cw 10.2.9

ラベル(1)
0 件の賞賛
返信
1 解決策
2,120件の閲覧回数
CrasyCat
Specialist III

Hello

If you ran CodeWarrior for StarCore V10.1.1 on the same host PC, you probably have the Jungo USB drivers still installed.

In order to remove the Jungo Driver and install the new USB drivers, follows the instruction in
   {Install}\SC\ccs\driver\usb\readme.txt

Where {Install} stands for your V10.2.9 installation directory.

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,121件の閲覧回数
CrasyCat
Specialist III

Hello

If you ran CodeWarrior for StarCore V10.1.1 on the same host PC, you probably have the Jungo USB drivers still installed.

In order to remove the Jungo Driver and install the new USB drivers, follows the instruction in
   {Install}\SC\ccs\driver\usb\readme.txt

Where {Install} stands for your V10.2.9 installation directory.

CrasyCat

0 件の賞賛
返信
2,120件の閲覧回数
hemah
Contributor I

Hi,

Now its working fine. Thanks a lot for your timely help.

--

Best Regards

Hema H

0 件の賞賛
返信