Problem loading MSC8156ADS board with cw 10.2.9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem loading MSC8156ADS board with cw 10.2.9

Jump to solution
2,792 Views
hemah
Contributor I

Im getting follwing error while i am trying to load a application in MSC8156ADs board using cw 10.2.9

Failed to resume target process., CCSProtocolPlugin : Could not connect to the probe (or other debug link)

 

The same application is loading without any error when i tried with cw 10.1.1

whether there is any settings that is to be changed in debug configurations while loading with cw 10.2.9

Labels (1)
0 Kudos
Reply
1 Solution
2,118 Views
CrasyCat
Specialist III

Hello

If you ran CodeWarrior for StarCore V10.1.1 on the same host PC, you probably have the Jungo USB drivers still installed.

In order to remove the Jungo Driver and install the new USB drivers, follows the instruction in
   {Install}\SC\ccs\driver\usb\readme.txt

Where {Install} stands for your V10.2.9 installation directory.

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
2,119 Views
CrasyCat
Specialist III

Hello

If you ran CodeWarrior for StarCore V10.1.1 on the same host PC, you probably have the Jungo USB drivers still installed.

In order to remove the Jungo Driver and install the new USB drivers, follows the instruction in
   {Install}\SC\ccs\driver\usb\readme.txt

Where {Install} stands for your V10.2.9 installation directory.

CrasyCat

0 Kudos
Reply
2,118 Views
hemah
Contributor I

Hi,

Now its working fine. Thanks a lot for your timely help.

--

Best Regards

Hema H

0 Kudos
Reply