Issue with fopen()/malloc() function in CW v3.0 (CW IDE version 5.7.0) in 8144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with fopen()/malloc() function in CW v3.0 (CW IDE version 5.7.0) in 8144

7,924 Views
kanu__
Contributor III

hi ,

 

I am using code warrior 3.0 for my project. 

In that i am using fopen functionality. 

 

While debugging , when it enters the first  fopen() after my 'int main()', no problem for my application (it works fine).

 

But at the second time (in a while loop) , when it enters in fopen(),  goes to the following function in msc814x_intr_vectors.asm file 

 

 

;Entry 5 Reserved    

jmp>___EmptyIntHandler  

 dup 29    

nop

 endm

 

When i traced the path , i found as , 

 

from fopen() in my application 

 

to

 

fopen() in C:\Program Files\Freescale\CodeWarrior\StarCore_Support\compiler\src\rtlib\expanded\fopen_common.c

 

to

 

__do_open() in C:\Program Files\Freescale\CodeWarrior\StarCore_Support\compiler\src\rtlib\expanded\fopen_common.c

 

to

 

malloc() in C:\Program Files\Freescale\CodeWarrior\StarCore_Support\compiler\src\rtlib\expanded\maloc_common.c

 

From this malloc() function it is going to the exception (finally stuck   ) goes to msc814x_intr_vectors.asmfile

 

Here am pasting the code stuff of malloc() stuck area (Inside the while() loop )from the maloc_common.c

 

 

 

/* First: attempt to allocate the buffer from the existing pool with a

     minimum of wasted space. */

while ( NULL != p )

{

  if ( NO == p->used && nbytes <= p->size && waste > ( p->size - nbytes ) ) => throws exception from this area 

  waste = p->size - nbytes, best_fit = p;


  p = p->lnk;  

  }

 

 

I don't know why this happens in the second time when fopen()  calls.

Can any one help me out in solving this problem?

This is the whole issue .

 

/renjith_g

Labels (1)
Tags (1)
0 Kudos
Reply
9 Replies

5,037 Views
J2MEJediMaster
Specialist I

The empty interrupt handler is a catch-all for when the program gets lost and is out in the weeds. The fact that fopen() works initially but dies in a loop makes me thing that your loop code is doing something that makes fopen() run out of memory (hence the malloc() call). What does your loop code look like?

 

---Tom

0 Kudos
Reply

5,037 Views
kanu__
Contributor III

 

hi,

 

It is my custom embedded application taking some memory.Also how can prevent this exception at fopen()? ( or how can i give enough / more memory fopen() ?) 

How can i find/control the memory overflow ?

 

/Kanu__

0 Kudos
Reply

5,037 Views
J2MEJediMaster
Specialist I

If you comment out the fopen() in the loop, does the program work, as much as can be expected without the use of that function? The fact that you say the fopen() fails to work in the loop yet works outside of the loop, makes me think that something in the loop code is the culprit. Somehow it's creating a memory leak, or perhaps calling fopen() so often that you run out of memory.

 

---Tom

0 Kudos
Reply

5,037 Views
kanu__
Contributor III

 

hi,

 

The application is very well depend on the fopen() call. So not able to realize without it.

As like your suggestion , may be my loop code is having some leakage.

 

Now am analyzing that.

 

Which are all places , should i give more importances to find the leakage? 

 

What are the memory constraints in board /simulator? 

 

/Kanu__

0 Kudos
Reply

5,037 Views
kanu__
Contributor III

 

No other replies yet?

 

/Kanu__

0 Kudos
Reply

5,037 Views
CrasyCat
Specialist III

Hello

 

Did you check the sample project in {Install}/(CodeWarrior_Examples)\StarCore_Examples\FileIO?

 

As far as I know they are using fopen.

 

CrasyCat

0 Kudos
Reply

5,037 Views
kanu__
Contributor III

 

hi ,

yes i tried the three example projects in the above directory.

They are working fine and completed successfully.

 

/Kanu__

 

 

 

0 Kudos
Reply

5,037 Views
Irene
NXP Pro Support
NXP Pro Support

Did you make sure that you increase the heap this is what affects the fopen() function?

0 Kudos
Reply

5,037 Views
kanu__
Contributor III

hi,

 

Can you please  describe a little bit more on that , ie heap memory which is relating with fopen()?

I haven't  touched the heap size control parameter in my code /configuration file .

 

Also from where i need to start my debugging ?

/Kanu__

0 Kudos
Reply