Interface function IMWprotocol::GetPreference is unimplemented

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interface function IMWprotocol::GetPreference is unimplemented

3,554 次查看
lorin
Contributor I

Hi,

 

My cw version is SC 10.1. I used it to debug m8156 ADS targets. it was running correctly before.

but today after I launch a debug configuration, it says

Exception occurred during launch.

Reason:Interface function IMWprotocol::GetPreference is unimplemented

 

What is this error mean?

Thanks!

 

/Lorin

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,424 次查看
Irene
NXP Pro Support
NXP Pro Support

Are you connecting to MSC8156ADS board?   How are you connecting to the target - USBTap or EthernetTAP? Can you send us the .log file that is located <workspace_folder>? 

 

What happens if you try to debug after you have clean and rebuild the project?

 

 

2,424 次查看
lorin
Contributor I

Hi,

I\m using the USB-Tap to connect the MSC8156ADS board.

it always stops at the same error when i start the dubug configuration.

 

thanks for the help~

 

 

0 项奖励
回复