Error while building project in codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while building project in codewarrior

4,057 Views
nxpram
Contributor I

Hi all,

We are facing below error while building project after importing. We are currently using  CodeWarrior Development Studio for StarCore 3900FP DSP v10.9.0 evaluation version. License is also placed in SC folder inside installation folder. We are trying use debugger mode.

Error:


**** Build of configuration C_Debug_8156_HW for project LTE-ASIC ****

C:\Freescale\CW_SC_3900FP_v10.9.0_1\gnu\bin\mingw32-make.exe -j32 all
'Building target: LTE-ASIC.eld'
'Executing target #1 LTE-ASIC.eld'
'Invoking: StarCore C/C++ Linker'
"C:/Freescale/CW_SC_3900FP_v10.9.0_1/SC/StarCore_Support/compiler/bin/scc" -F "LTE-ASIC.args" -o "LTE-ASIC.eld"
[SCC,1,1407,-1]:WARNING: Option -env $(SCEnvironmentEnv) is invalid, ignored: $(SCEnvironmentEnv) is invalid, ignored
[SCC,2,1605,-1]:ERROR: Cannot find license file.
mingw32-make: *** [LTE-ASIC.eld] Error 1

Please help us here. Thanks in advance.

@codewarrior @starcore @c++

0 Kudos
Reply
1 Reply

4,044 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you said that you use evaluation license, I suppose that the the evaluation license of CW tools has expired, which leads to the fact that the CW does not start the compiling.

In the case, pls download another evaluation version of CW tools again or order the license from the link:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply