Error while building project in codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while building project in codewarrior

4,063件の閲覧回数
nxpram
Contributor I

Hi all,

We are facing below error while building project after importing. We are currently using  CodeWarrior Development Studio for StarCore 3900FP DSP v10.9.0 evaluation version. License is also placed in SC folder inside installation folder. We are trying use debugger mode.

Error:


**** Build of configuration C_Debug_8156_HW for project LTE-ASIC ****

C:\Freescale\CW_SC_3900FP_v10.9.0_1\gnu\bin\mingw32-make.exe -j32 all
'Building target: LTE-ASIC.eld'
'Executing target #1 LTE-ASIC.eld'
'Invoking: StarCore C/C++ Linker'
"C:/Freescale/CW_SC_3900FP_v10.9.0_1/SC/StarCore_Support/compiler/bin/scc" -F "LTE-ASIC.args" -o "LTE-ASIC.eld"
[SCC,1,1407,-1]:WARNING: Option -env $(SCEnvironmentEnv) is invalid, ignored: $(SCEnvironmentEnv) is invalid, ignored
[SCC,2,1605,-1]:ERROR: Cannot find license file.
mingw32-make: *** [LTE-ASIC.eld] Error 1

Please help us here. Thanks in advance.

@codewarrior @starcore @c++

0 件の賞賛
返信
1 返信

4,050件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you said that you use evaluation license, I suppose that the the evaluation license of CW tools has expired, which leads to the fact that the CW does not start the compiling.

In the case, pls download another evaluation version of CW tools again or order the license from the link:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信