Error launching external scanner info generator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error launching external scanner info generator

3,219 次查看
hoaho
Contributor I

Dear all,

I have just used code warrior studio Development studio for power architecture (CW for PA ) and I tried to import a project. I have built the project many times and it was successful...

However, when I uninstall the CW for PA, re-install it and imported the project. The window of problems displays some errors and warnings as:

DescriptionResourcePathLocationType
mingw32-make: *** [memory_sharing/sources/memory_sharing.o] Error 1engineC/C++ Problem
mingw32-make: *** Waiting for unfinished jobs....engineC/C++ Problem
mingw32-make: *** [engine/sources/engine.o] Error 1engineC/C++ Problem
mingw32-make: *** [engine/sources/sender.o] Error 1engineC/C++ Problem
Error launching external scanner info generator (F:/CW_PA_v10.4.0/Cross_Tools/gcc-4.8.2-XMe500v2-linuxspe/bin/powerpc-unknown-linux-gnuspe-gcc -E -P -v -dD F:/workspace_PA/.metadata/.plugins/org.eclipse.cdt.make.core/specs.c)engine[Discovery Options] page in project propertiesC/C++ Problem
Cannot run program "F:\CW_PA_v10.4.0\Cross_Tools\gcc-4.8.2-XMe500v2-linuxspe\bin\powerpc-unknown-linux-gnuspe-gcc" (in directory "F:\workspace_PA\engine"): CreateProcess error=2, The system cannot find the file specifiedengine[Discovery Options] page in project propertiesC/C++ Problem

 

I don't understand what is the problem? Because I have built the project many times by CW for PA before... and all of them were successful!

In addition, When I run another project, it built successfully.

Can you figure out the problem for me!

Many thanks!

标签 (1)
0 项奖励
回复
2 回复数

2,471 次查看
lunminliang
NXP Employee
NXP Employee

Hello Hoa Ho,

Did you have all the project file saved and imported? Also its' included path?

And it seems your project is CodeWarrior Linux Project, isn't it? Do you have it's corresponding service pack installed also? If not please do this from:

"Help"->"Install New Software"->“Work with: FSL PA Build Tools...”->"PA GCC 4.8.2 - r963 Build Tools Service Packs"->"Service Pack for Windows GccE500mcLinux Build Tool version 4.8.2-r963".

Why do you need to reinstall your CodeWarrior?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,470 次查看
hoaho
Contributor I

Dear lunmiliang,

First, Many thanks for your answer.

I agree with you that the project haven't had enough files yet. I have just solved the problem.

I wanted to test a demo project on BSC9132 board. Having some errors when I fix the source code.

So I reinstalled the soft! ^^

0 项奖励
回复