Do breakpoints affect code speed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do breakpoints affect code speed?

Jump to solution
2,337 Views
tim79
Contributor I

We have code that monitors if our data is being processed fast enough, and asserts if it is not. Without breakpoints, the code runs fine. If I add a breakpoint to critical areas, the code asserts, even if its a conditional breakpoint that never gets hit. This seems to indicate adding breakpoints slows down execution of the code. Is this the case?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,037 Views
Daniel_Popa
NXP Employee
NXP Employee

 

 

 

Hi Tim,

 

 

 

The behavior for conditional breakpoints that you are seeing (speed slow down) is correct, because, even if the breakpoint is not hit (condition = TRUE), the condition needs to be evaluated each time the PC reach that region. For this, the debugger halts the core, check the condition and if it is FALSE then execute the next piece of code.

 

 In this mode the IDE is not notified about the debugger action and the user has the feeling that everything runs permanently.

 

If you really want to make sure about this aspect you can open the CCS console and you can enable the logging (log v). You will see some interaction between the DSP and the CW where the conditional breakpoints are checked.

 

View solution in original post

0 Kudos
Reply
1 Reply
2,038 Views
Daniel_Popa
NXP Employee
NXP Employee

 

 

 

Hi Tim,

 

 

 

The behavior for conditional breakpoints that you are seeing (speed slow down) is correct, because, even if the breakpoint is not hit (condition = TRUE), the condition needs to be evaluated each time the PC reach that region. For this, the debugger halts the core, check the condition and if it is FALSE then execute the next piece of code.

 

 In this mode the IDE is not notified about the debugger action and the user has the feeling that everything runs permanently.

 

If you really want to make sure about this aspect you can open the CCS console and you can enable the logging (log v). You will see some interaction between the DSP and the CW where the conditional breakpoints are checked.

 

0 Kudos
Reply