Debug Memory View - Export/Inport

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Memory View - Export/Inport

ソリューションへジャンプ
3,464件の閲覧回数
ITCO00
Contributor III

Hello,

 

I'm using CW 10.1.3 for SmartDSP with SDOS. In the debug Memory View I do the following:

1. I export (dump) 2KB of memory data from DDR1 location to a raw binary file. This operation is OK.

2.  Then, I overwrite the first few memory locations with 0xFF,

3. Finally, I try to import the file I previously exported to the beginning of the memory location.

The Import operation does not work. If I reduce the data size to 1KB, it works OK.

In any case I've checked the exported file, and its content was correct.

What might be the problem?

 

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,415件の閲覧回数
Irene
NXP Pro Support
NXP Pro Support

Have you tried to import/export memory using Target Task option?

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,415件の閲覧回数
Irene
NXP Pro Support
NXP Pro Support

Have you tried to import/export memory using Target Task option?

0 件の賞賛
返信
2,415件の閲覧回数
ITCO00
Contributor III

Hi,

 

Thanks, I wasn't aware of this option. I've tried to create Target Task for Fill, Export and Import Memory, using hex data and physical memory, and it works fine.

 

thank you.

 


0 件の賞賛
返信