CodeWarrior for MCU Version: 10.2 and Quick_Start_r2.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for MCU Version: 10.2 and Quick_Start_r2.6

1,225 Views
marekdobrovsky
Contributor I

Hi,

I use CodeWarrior for MCU Version: 10.2 and I program MC56F84 with Quick_Start_r2.6.

A program that I am working on uses a number of arrays to hold various items such as time, date, etc.

I created project as follow:

 

  1. 4.1 Creating a new project

To create a new project based on the DSC56800EX_Quick_Start project templates (stationery), two options are available:

• Standalone C-application - all essential driver files are located in the project folder.

• C-application - driver files are linked to the project from DSC56800EX_Quick_Start depository.

Following steps suppose DSC56800EX_Quick_Start to be installed in a default installation folder

c:\Freescale\DSC56800EX_Quick_Start_X_Y to link properly driver files when the new project is based on C-application template.

Creating a new project based on QuickStart C-application template:

  1. 1. Launch CodeWarrior IDE from the Start->Programs->Freescale CodeWarrior menu and open

existing or create new Workspace.

  1. 2. Choose File->Import command and select General->Existing Projects into Workspace and click on Next.

 

If I debug, there is a problem with initial of arrays or variables, all of this are zero (photo is attached). What do I have to do for correct initial.

 

Thank you very much for your advice


21801_21801.jpgarray.jpg

Labels (1)
0 Kudos
Reply
0 Replies