CW 10.1.8 SC3000-ld error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.1.8 SC3000-ld error

ソリューションへジャンプ
3,162件の閲覧回数
ITCO00
Contributor III

Hi,

 

I try to buil my project in the CW 10.1.8. and receive LINK error, sc3000-ld fails. An Error Window (WinXP) is received (see attached file).

CW Error details:

Error code is: [SCC,2,1027,-1] 

Message is:

ERROR: Non-zero return status from "C:\Program Files\Freescale\CW SC v10.1\SC\StarCore_Support\compiler\bin\sc3000-ld.exe"

 

This problem occures also when creates a new CW project and build it.

 

What might cause this problem?

 

ITCO

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,539件の閲覧回数
CrasyCat
Specialist III

Hello

 

I would recommend you to submit a service request for that.

Click here to submit a service request.

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,540件の閲覧回数
CrasyCat
Specialist III

Hello

 

I would recommend you to submit a service request for that.

Click here to submit a service request.

CrasyCat

0 件の賞賛
返信
2,539件の閲覧回数
ITCO00
Contributor III

Hello,

 

Since I'am tight with my schedual, I've uninstall the CW, and re-install it again, and the probelm has disappeared.

I think that, since preior to 10.1.8, I've installed in my computer CW 10.1.3, but never uninstalled it, and this might be the problem.

Anyway, I'll send SR on this issue in case that my susspecious is not real.

 

ITCO

0 件の賞賛
返信