[CW 10.1.8] Error when including breakpoint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[CW 10.1.8] Error when including breakpoint

ソリューションへジャンプ
2,614件の閲覧回数
Lo
Contributor I

Hi,

 

I am trying to debug an application but for some reasons, CW crashes when I include a breakpoint at a specific location.

When i remove this breakpoint (but some others still stand), the application runs with no problem.

Do you have any idea of the cause ?

Hereafter the screenshots of the displayed error and the dumpfile.

 

Thank you

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,200件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you look at following article?

      http://www.eclipsezone.com/eclipse/forums/t61566.html

 

It provides some tricks on how to clean up a workspace.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,200件の閲覧回数
Lo
Contributor I

Hi,

 

Last time, the problem dissapeared suddenly after a while but I still got some problems...

 

When an error occurs during debug with a crash (screenshots attached to the previous post: 3 consecutive error messages), the project seems to be corrupted after that.

After restart, the runs crash if I try to stop at some breakpoint.

I need then to create a new workspace to avoid this problem and it takes time.

I guess there is a way to clean the workspace and i've found a link but it doesn't work for me.

 

http://blogs.freescale.com/2011/11/10/codewarrior-tool-tip-1-improve-performance-by-cleaning-house-i...

 

Thank you for your help

0 件の賞賛
返信
2,201件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you look at following article?

      http://www.eclipsezone.com/eclipse/forums/t61566.html

 

It provides some tricks on how to clean up a workspace.

 

CrasyCat

0 件の賞賛
返信