Ask a few questions about the MSC8157 SmartDSP operating system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ask a few questions about the MSC8157 SmartDSP operating system

5,639 Views
819277784
Contributor II

Hi:

When I recently used the MSC8157, I needed to use the SmartDSP operating system, but I encountered the following problems when using the operating system:

(a): When I run SmartDSP early, the system will be stuck in the function ‘osWaitForAllCores();’. When I redefine       OS_MULTICORE = OFF, OS_MULTICORE_SYNCHRONIZATION = OFF, the system will run normally.

(b):I created a simple task under the SmartDSP operating system. The source code is as follows. The problem is that after       the system initialization completes all the operations, my task will not be executed. I have seen the SmartDSP OS Usrt       Guide and the SmartDSP OS API Reference. Manual two documents, and found no mistakes, please advise, thank you       very much:

      

os_task_handle             Test_Task1_Handle;            
os_task_init_param_t    Test_Task1_Para;                
unsigned char *Test_TASK1_STACK;                        
#define Test_TASK1_STACK_SIZE                4096    

void Test_Task1_Function(unsigned long p)
{
    while(1)
    {
        printf("My Name is Test_Task1_Func\r\n");
        osTaskDelay(500);
    }
}

void Test_Task1_Create(void)
{
    os_status status;
    status = osTaskFind(&Test_Task1_Handle);
    OS_ASSERT_COND(status == OS_SUCCESS);
    
    Test_TASK1_STACK = osMalloc(Test_TASK1_STACK_SIZE,OS_MEM_LOCAL);
    Test_Task1_Para.task_function = Test_Task1_Function;            
    Test_Task1_Para.task_arg = (os_task_arg)osGetDeviceID();        
    Test_Task1_Para.top_of_stack = (unsigned long)Test_TASK1_STACK;            
    Test_Task1_Para.stack_size = Test_TASK1_STACK_SIZE;            
    Test_Task1_Para.task_flags = 0;                                
    Test_Task1_Para.task_priority = OS_TASK_PRIORITY_12;            
    Test_Task1_Para.task_name = "Test_TASK1";                        
    Test_Task1_Para.private_data = 0;                            
    Test_Task1_Para.init_stack = TRUE;                            
    
    osTaskCreate(Test_Task1_Handle,&Test_Task1_Para);                
}

void main()
{
    os_status status;   // The only local variable in main()

    /* OS Initialization - call before any other OS API calls. */
    status = osInitialize();
    if (status != OS_SUCCESS) OS_ASSERT;

    /* Interrupts are disabled until osStart() is called.
       You must not enable interrupts at this point !!! */

    /* Place any required initialization code within appInit().
       Using local variables inside main() is NOT recommended, because
       its stack is never restored - osStart() never returns !!! */
    status = appInit();
    if (status != OS_SUCCESS) OS_ASSERT;
    
    Test_Task1_Create();
    
    /* Start the OS with the background task. OS ticks now start.
       appBackground() should not return unless there is an error. */
    status = osStart(appBackground);
    if (status != OS_SUCCESS) OS_ASSERT;

    /* Execution reaches this point only if an error occurs. */
}

Labels (1)
0 Kudos
Reply
4 Replies

5,489 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HaiFeng,

I have asked AE team, I will give you a reply shortly after I get a feedback.

BR

Xiangjun Rong

0 Kudos
Reply

5,489 Views
819277784
Contributor II

Ok, thank you very much.

0 Kudos
Reply

5,489 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HaiFeng,

This is AE team reply:

"

This is an update to your question/request:

 

  1. a) to run the multi-core project , you should operate with those milticore icons, like 'multicore resume', 'multicore suspend'... Please refer to the 'Targeting Starcore DSP.pdf' in your CW installation folder
  2. b) Do you mean your test_task1 is not run?

     IN SDOS, to  make a task run, you need the following to trigger scheduler,

      - the current running task yield itself

      - interrupt happens and responed

    Please check your code to ensure the above. Also you can study the SDOS basic_demo or stationary demo project

"

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

5,489 Views
819277784
Contributor II

Hi,XiangJun:

        Thanks for your help.The second question has been solved. Now I will go to the document mentioned above and try to solve the first problem. Thank you very much.

0 Kudos
Reply