which Special Edition: CodeWarrior (the Free Version) will Support QCVS 4.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

which Special Edition: CodeWarrior (the Free Version) will Support QCVS 4.1?

3,654件の閲覧回数
nadavganor
Contributor I

i am loking for a free version of CodeWarrior the will support QCVS 4.1same as Eclips.

can you recommend?

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,189件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Nadav,

The QCVS is available on

          for CodeWarrior for ARM v7 10.0.3 or  higher version

          for CodeWarrior for Power Architectures 10.3 or  higher version

Are you looking for a Classic version ?

      CodeWarrior Development Tools for PowerQUICC|Freescale

Under classic the QCVS is not available.

For details, please have a look to:

        Processor Expert Software: QorIQ Configuratio|Freescale


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,189件の閲覧回数
nadavganor
Contributor I

Hi Pascal Irrle


I already know this versions works i am looking for a free version that can support QCVS

maybe one of the Special Edition see link:

Special Edition Software|Freescale


Thanks

Nadav

0 件の賞賛
返信

3,189件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Nadav,

what is the architecture you're looking for ?


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,189件の閲覧回数
nadavganor
Contributor I

Hi

i amusing the QCVS for doing the configuration word for AT4 (T4080/T4160/T2080)

and for activating the last version of the QCVS we need CW

i don't want to purchase the CW program because i don't exactly need it i just need the QCVS

if there any free Software (not a trial) that can run the QCVS i will be glad to know about here

Thanks

0 件の賞賛
返信

3,189件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please take a look on http://www.freescale.com/webapp/sps/download/mod_download.jsp?colCode=QCVS_OFFLINE-ECLIPSE-3.7-4.2&l...

This is the qcvs version for stock eclipse(3.7 or 4.2).

Adrian

0 件の賞賛
返信

3,189件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi Nadav,

Yes, CodeWarrior Development Studio v10 for Power Architecture® Technology (Eclipse) has free Special Edition. It's full featured 30-day evaluation copies also available via download. Includes all features listed under Professional License.

It's available from the link below, click "Download Evaluation" button.

CodeWarrior Dev Tools for Power Architecture|Freescale

0 件の賞賛
返信

3,189件の閲覧回数
nadavganor
Contributor I

Hi,

I have the CodeWarrior Development Studio v10 and its work perfectly for QCVS but its 30-day trial and i am looking for a freeware same as Eclipse .

do you have any Suggestions ?

0 件の賞賛
返信

3,189件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Nadav,

We don't have special edition for CW for PA v10.x.

      CodeWarrior Development Suites|Freescale

At left select QorIQ Power Architecture (Eclipse IDE)


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信