whether S70GL02GS NOR Flash programming support available in Codewarrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whether S70GL02GS NOR Flash programming support available in Codewarrior?

ソリューションへジャンプ
2,778件の閲覧回数
karunakaranradh
Contributor IV

In code warrior 10.4.0 does not have S70GL02GS NOR flash device support in flash programming task.

 

Any Latest code warrior have S70GL02GS NOR flash device support support?

or

How to create the S70GL02GS device support for flash programming?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,183件の閲覧回数
karunakaranradh
Contributor IV

Hi Lunmin,

Thanks for your reply.

I taken s29gl01 file as reference.

change only sector size as 2048 and choose 64Mx16x1memory organization.

With this configuration, it was working fine.

Regards

Karunakaran R

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,183件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

CW10.4.0 is the latest version till now, the above flash device is not supported.

Basically most of the common flash algorithm is supported by the programmer in CW tool. For creating the above device support for flash programming, you could refer to the application note AN4948 and below thread as well:

Flash Programmer for CodeWarrior Power Architecture

Adding a new Flash Device to Codewarrior 10.x


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,184件の閲覧回数
karunakaranradh
Contributor IV

Hi Lunmin,

Thanks for your reply.

I taken s29gl01 file as reference.

change only sector size as 2048 and choose 64Mx16x1memory organization.

With this configuration, it was working fine.

Regards

Karunakaran R

0 件の賞賛
返信