uart0 console;messy code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uart0 console;messy code

1,823 Views
连营张
Fresh Out Contributor

hello,i'm working on the p2041rdb.i reflashed the p2041rdb NOR flash image(QorIQ_SDK_V1.4_P2041RDB_20130625_NOR_Flash.bin),after that i found the uart0 console don't print boot message,only showing messy code.that's why?please help me.the serial baud rate is 115200,none flow control.

Labels (1)
0 Kudos
Reply
2 Replies

1,674 Views
连营张
Fresh Out Contributor

i guess that the uart0 is corrupted.can i redirect the boot messages to uart1?

0 Kudos
Reply

1,674 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please create a CodeWarrior bareboard sample project, and execute this project, as normal you will see "Hello CodeWarrior!" from UART0 after executing this program. This could help you to make decision whether it is the problem of image or UART0 on the target board.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply