twrmp55125 linker error with printf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

twrmp55125 linker error with printf

2,153件の閲覧回数
stevasway
Contributor III

I got a twrmpc5125 board, with a TWR SER board.

I'm using MQX OS, with its libraries.

I have no problem with printf in other C modules, but when I add an additional module (with printf inside) I found:

 

Link error: Undefined: 'InitializedUART' Referenced from '__init_uart_console' in MSL_C.PPCEABI.bare.H.a

...

 

Where am I wrong?

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,669件の閲覧回数
J2MEJediMaster
Specialist I

 I assume that the printf statements that work use a MQX library? And this new module is a bunch of code you pulled in from elsewhere? The error message points out that the new module is trying to use a bare-board implementation of the printf function, where bare-board means: "no OS, access the metal directly". If you're using the MQX OS to print, you need to modify the new module to call its printf function.

 

---Tom

0 件の賞賛
返信