the hardware breakpoint can't be hit in debugging windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the hardware breakpoint can't be hit in debugging windows

1,328 Views
joshuali
Contributor I
Category: Technical Request Topic: CodeWarrior Target: PowerQUICC (8xx, 82xx, 83xx, 8 Product: CW for Power Architecture Root Cause/Nature: Feature Request RTOS: Embedded Linux Major: 8 Minor: 8 Patch: 3 Component: Debugger Host: Win XP Type: Query Defect/Enhance #: - Severity: Critical Subject:

the hardware breakpoint can't be hit in debugging windows

the board is MSC8144ADS  From freescale,cpu is MPC8560

Description:

When I Debug the U-Boot Bootstrap Firmware following the step on Pro & Linux App Edition Targeting Manual.pdf page 210,it's seemed everything is ok , but when I set hardware breakpoint in debugging windows, then run it,the breakpoint is not be hit,I want to know what's maybe wrong? 

When create new project with 8144ads template to debug,the hardware breakpoint is ok to hit, 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

734 Views
J2MEJediMaster
Specialist I

I am not sure on what you are asking here. Is this supposed to be an actual feature request? If so, you need to enter it through the Service Request page.

 

---Tom

0 Kudos
Reply