spi flash u-Boot parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

spi flash u-Boot parameters

7,215 Views
nareshpuli
Contributor III

Hello,

we are using NxpP2020RDB, Please can you attach Bootcommands for SPI_Flash.

what are parameters needed to configure for SPI_Flash kernel Boot-up

My U-Boot Log

 sf probe 0
SF: Detected S25FL128P_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB

 printenv
baudrate=115200
bdev=sda1
bootcmd=setenv bootargs root=/dev/$bdev rw rootdelay=30 console=$consoledev,$baudrate $othbootargs;usb start;ext2load usb 0:1 $loadaddr /boot/$bootfile;ext2load usb 0:1 $fdtaddr /boot/$fdtfile;bootm $loadaddr - $fdtadr
bootdelay=10
bootfile=uImage
consoledev=ttyS0
ethact=eTSEC1
ethprime=eTSEC1
fdtaddr=c00000
hostname=unknown
hwconfig=usb1:dr_mode=host,phy_type=ulpi
jffs2nand=mtdblock9
jffs2nor=mtdblock3
loadaddr=1000000
map_lowernorbank=i2c dev 1; i2c mw 18 1 02 1; i2c mw 18 3 fd 1
map_uppernorbank=i2c dev 1; i2c mw 18 1 00 1; i2c mw 18 3 fd 1
nandboot=i2c dev 1; i2c mw 18 1 0xe8 1; i2c mw 18 3 0x03 1; reset
nandbootaddr=100000
nandfdtaddr=80000
netdev=eth0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdr
norboot=i2c dev 1; i2c mw 18 1 0xc8 1; i2c mw 18 3 0x03 1; reset
norbootaddr=ef080000
norfdtaddr=ef040000
pciboot=i2c dev 1; i2c mw 18 1 0xa8 1; i2c mw 18 3 0x03 1; reset
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs ramdisk_size=$ramdisk_size;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr
ramdisk_size=120000
ramdiskaddr=2000000
ramdiskfile=rootfs.ext2.gz.uboot
rootpath=/opt/nfsroot
sdboot=i2c dev 1; i2c mw 18 1 0x68 1; i2c mw 18 3 0x03 1; reset
spiboot=i2c dev 1; i2c mw 18 1 0x28 1; i2c mw 18 3 0x03 1; reset
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot; protect off 0x11001000 +$filesize; erase 0x11001000 +$filesize; cp.b $loadaddr 0x11001000 $filesize; protect on 0x11001000 +$filesize; cmp.b $loadaddr 0x11001000 $filesize
uboot=u-boot.bin

Environment size: 1908/8188 bytes

0 Kudos
Reply
2 Replies

4,499 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello naresh puli,

Please refer to the following procedure to boot jffs2 filesystem from SPI flash.

In Linux please run the following command to get mtd block information

root@p2020rdb:~# mtd_debug info /dev/<mtd block jffs2 for spi>
mtd.type = MTD_NORFLASH
mtd.flags = MTD_BIT_WRITEABLE
mtd.size = 524288 (512K)
mtd.erasesize = 65536 (64K)
mtd.writesize = 1
mtd.oobsize = 0
regions = 0

compare the "mtd.erasesize" with yocto "JFFS2_ERASEBLOCK" in the file meta-fsl-ppc/conf/machine/<platform>.conf and modify "JFFS2_ERASEBLOCK" according to "mtd.erasesize" 

Under u-boot, please configure the following bootargs.

=>setenv bootargs 'root=/dev/<mtd block for spi> rw rootfstype=jffs2 console=ttyS0,115200'
=>sf probe 0
=> sf read $loadaddr <kernel addr in SPI flash> <proper size for kernel>
=> sf read $fdtaddr <fdt addr in SPI flash> <proper size for fdt file>
=>bootm $loadaddr - $fdtaddr


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,499 Views
nareshpuli
Contributor III

Dear Yiping Wang,

i hope you are doing good.....

sorry for the late response

whatever i said i followed the same procedure but my spi flash can't get kernel image!

setenv bootargs 'root=/dev/mtd block14 rw rootfstype=jffs2 console=ttyS0,115200'

sf probe 0

sf read 0x1000000 0x00180000 0x404e56
sf read 0xc00000 0x00100000 0x3570

bootm 1000000 - c00000

Environment size: 1984/8188 bytes
=> setenv bootargs 'root=/dev/mtd block14 rw rootfstype=jffs2 console=ttyS0,115200'
=> sf probe 0
SF: Detected S25FL128P_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
=> sf read 0x1000000 0x00180000  0x404e56
SF: 4214358 bytes @ 0x180000 Read: OK
=> sf read  0xc00000 0x00100000  0x3570
SF: 13680 bytes @ 0x100000 Read: OK
=> bootm 1000000 - c00000
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at 01000000 ...
   Image Name:   Linux-3.12.19-rt30-QorIQ-SDK-V1.
   Created:      2016-10-26   5:50:59 UTC
   Image Type:   PowerPC Linux Kernel Image (gzip compressed)
   Data Size:    4214294 Bytes = 4 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!

0 Kudos
Reply