config JTAG chain (P1010 & mpc5125) in CW 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

config JTAG chain (P1010 & mpc5125) in CW 10

822 Views
robertapplebaum
Contributor I

Support-

I need to debug a P1010 but it is in a JTAG chain with an MPC5125.

How can I create the correct JTAG config file?

Codewarrior fails due to an unrecognized core.

 Is there an option for the 5125 in CW?

should I define it as GENERIC? with what jtag parameters please?

Thank you.

Robert

0 Kudos
Reply
1 Reply

612 Views
sinanakman
Senior Contributor III

Hi Robert

I wonder if your question is specifically for having P1010 and MPC5125 on the same chain or finding the right config for MPC5125. Were you able to connect to MPC5125 independently or are you also looking for a config file just to do this ? I thought if you clarify you might get more help here.

Regards

Sinan Akman

0 Kudos
Reply