simulator target on powerpc linux platform edition for powerpc 8548

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

simulator target on powerpc linux platform edition for powerpc 8548

2,311件の閲覧回数
Ratheesh
Contributor I
Hi all
        I am unable to connect to simulator target in the code warrior CodeWarrior for Power Architecture, Linux Platform Edtn (Linux) version 8.7. I am getting following message:
 
==================== ERROR LOG ======================
ccssim2ExecPath = "/usr/local/Freescale/CodeWarriorIDE/ccs/bin"
CONFIGURATION:* waiting for Clients (On Port=40969) ...
 
Allocated connection 0
 
Allocated device 0
 
Accepting : Device 0 : Type e500elf8
 
The current time is: Wed Sep 19 09:46:31 2007
 
This version of PowerPC ISS expired on: Mon May  7 10:29:59 2007
 

Please contact your PowerPC ISS support representative, and request
an updated release.  This version has expired in order to ensure
that you are provided with an accurate and updated version.
Please report the following expiration variable name to your
PowerPC ISS support representative: EXPIRATION_020B
 
ISS exited normally.
===========================================================
Kindly tell me what might be wrong and how to correct it?
 
Thanks and Regards
 
Ratheesh
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

927件の閲覧回数
Black
Contributor I
Do you have the release version of CodeWarrior PA 8.7 Linux Platform edition? Please go to <install_dir>/CodeWarriorIDE/CodeWarrior/CodeWarrior_Plugins/Support/Products; You can read the version and build number in the xml files found in this folder. It should be build 70322.
 
You can get the 8.7 release version from here.
 
Then please check you license file located in $INSTALL_DIR/CodeWarriorIDE/CodeWarrior/license.dat.
 
If it has expired please contact our licensing department at [email protected] for a permanent license.
I hope this helps.
0 件の賞賛
返信