"Core not responding" when programing MPC8377

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Core not responding" when programing MPC8377

ソリューションへジャンプ
2,503件の閲覧回数
alerk03
Contributor I

I'm using codewarrior windows version to program MPC8377. The codewarrior version is the newest 8.8.2. I use M29W640GT flash instead of S29GL064R3 on board. But error happens when programing flash like:

Programming 0x00010000 bytes of Target Memory at 0xFE000000
Programming 0x00010000 bytes of Target Memory at 0xFE010000
Programming 0x00010000 bytes of Target Memory at 0xFE020000
Programming 0x00010000 bytes of Target Memory at 0xFE030000
Programming 0x00010000 bytes of Target Memory at 0xFE040000
Programming 0x00010000 bytes of Target Memory at 0xFE050000
Programming 0x00010000 bytes of Target Memory at 0xFE060000
Programming 0x00010000 bytes of Target Memory at 0xFE070000
Programming 0x00010000 bytes of Target Memory at 0xFE080000
Programming 0x00010000 bytes of Target Memory at 0xFE090000
Programming 0x00010000 bytes of Target Memory at 0xFE0A0000
Flash Programmer: CCSProtocolPlugin : Failed to continue thread [Core not responding]

 

The stop address will change every time. And I can use u-boot to program flash correctlly. So it seems that something is wrong with codewarrior or USBTAP. Could someone helps me to solve the problem?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,450件の閲覧回数
ronco
NXP Employee
NXP Employee

In situations like this, where flash-programming fails for no discernable reason, I find that slowing the Interface Clock Frequency of the USB TAP or Ethernet TAP usually helps.  From the CodeWarrior IDE Toolbar select Edit->Preferences->Remote Connections.  Double-click on the connection option you're using in the Flash Programmer. In the configuration panel that pops up, change the Interface Clock Frequency option to 1MHz.  You may find that faster speeds also work but start with 1MHz.

 

-Ron

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,451件の閲覧回数
ronco
NXP Employee
NXP Employee

In situations like this, where flash-programming fails for no discernable reason, I find that slowing the Interface Clock Frequency of the USB TAP or Ethernet TAP usually helps.  From the CodeWarrior IDE Toolbar select Edit->Preferences->Remote Connections.  Double-click on the connection option you're using in the Flash Programmer. In the configuration panel that pops up, change the Interface Clock Frequency option to 1MHz.  You may find that faster speeds also work but start with 1MHz.

 

-Ron

0 件の賞賛
返信